This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: driver vital signs demo gui choice Back or Front

Part Number: IWR1642BOOST

Hi,

May I ask whether the selection of xwr1642_profile_VitalSigns_20fps_Back/Front is related to whether the person is right or back to the board, or whether the board is right or back to the person's chest?

Best regards

  • And I also want to ask, if I want to measure an animal, can I put it on the back of the animal? Does it have any limitations? xwr1642_profile_VitalSigns_20fps_Back or Front?
    Looking forward to your reply.

  • Hi,

    The configuration is dependent whether the sensor is mounted on the front or back of the person. Antenna on the board always need to face the person for correct vital signs measurement.

    You can use the sensor to measure the vitals of the animal provided it is in the range supported by the demo. This demo is tuned for human vital signs detection i.e. maximum breath rate of 30 breaths per minute and 120 heart beats per minute. Demo cannot support beyond that.

    Regards