This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: IWR6843ISK

Part Number: IWR6843ISK
Other Parts Discussed in Thread: IWR6843,

Iam using  Hardcode config project which by default loads the configuration and  the point cloud data is pumped over XDS100 data port. I need to receive data over J5 connector pin5 (TX pin from IWR6843)of mmwave IC boost board. do we need to modify the code ?  Following switch settings are done mmwave boost board S7-off S8-ON . In IWR6843ISK board  switch S1-5 is off.do we need to do any other changes ?thanks