Other Parts Discussed in Thread: IWR6843,
Iam using Hardcode config project which by default loads the configuration and the point cloud data is pumped over XDS100 data port. I need to receive data over J5 connector pin5 (TX pin from IWR6843)of mmwave IC boost board. do we need to modify the code ? Following switch settings are done mmwave boost board S7-off S8-ON . In IWR6843ISK board switch S1-5 is off.do we need to do any other changes ?