I have a very similar issue to the link below.
I also use IWR6843AOPEVM (Rev. G) + DCA1000 + mmWave studio 02.01.01.00.
A few months ago I could use these two boards to receive signals on mmwave studio. But now I have changed to a laptop, and mmwave studio shows that it Unable to read FPGA Version. [error -5].
I did reflash the FPGA in the DCA1000, disable Firewall and make sure Ethernet static IP correct. They did not solve the issue.
But I don't seem to have hardware issues, the LED looks like everything is fine.
Images are the LED light after connected, mmwave studio error message, cf.json file in the postproc file.
led.pdferror.pdfcf.json dokument.pdf
Are there any other methods I can try?