Other Parts Discussed in Thread: PGA460, TUSS4470
Looking for piezo cermaic transducers for liquid level sensing if a few different freqs but having trouble finding them. I'm looking for a few different piezo ceramic disks with a high Q factor with resonant freqs in in the 40khz, 200khz, and 450-480khz. Do you have any suggestions on where to source these? I have already checked this out the TI List of example transducers. I've mostly been looking at piezo disks on Steminc which is references in some of the App Notes:
https://www.steminc.com/PZT/en/
However, that website is the single worst product website I've used and I haven't found a good alternative. They have no way to sort products by frequncey or mode of vibration. When you do find a product that will work after manually clicking on every option it's usually out of stock and also doesn't list parameters such as max drive voltage and max number of pulses for the piezo. Almost all the piezo disks on the site are listed as "Radial mode vibration application" and I'm looking for thickness mode vibration which for disk (as I understand it), should perform much better than radial mode because of the large surface area relative to the thickness making is more senative and easier to create sound pressure waves. I assume there is no issue using a piezo labled "radial mode transducer" in the axial/thickness mode if you can figure out the correct resonant freq of the thickness. How can I figure out the resonant axial frequencey of a piezo disk which is listed as "Radial mode vibration application"? For example:
https://www.steminc.com/PZT/en/piezo-ceramic-disc-10x3mm-r-215-khz
In the following app note:
when reccomending 1MHz transducer the note says "All of the transducers are approximately 2 mm thick. This is due to the requirement of axial (thickness) resonance mode of 1 MHz for these applications". What should the thickness of the disk be for it to be resonant at the following freqs: 40kHz, 200kHz, and 250-280kHz? Can you share how to calculate that so I can find what piezo ceramics will work in axial mode for the freqs I'm looking for?