Hi,
According to the angle resolution formula,
when θ=0,in the horizontal direction, the azimuth resolution is 9.549 degrees ,in the vertical direction,the elcvation resolution is 17.9049 degrees.From the above, we can see that the resolutions are low int the both directions. Now we encounter a problem:
In the following scene,
by experiment, the radar can not distinguish the sign and guard bar. Is it because the poor angle resolution in the horizontal and vertical directions? Is there any method to improve the angle resolution?
Thanks,
BR
Rata