This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Can the configurations of Phase shifter be saved in AWR2243 during switch between TDM-MIMO and beamforming?

Part Number: AWR2243

Dear team,

We use a MCU to configure the AWR2243 four-cascaded chip.

Now TDM-MIMO and beamforming have been set to AWR2243 and it works very well. And we can switch mode between TDM-MIMO and beamforming based on sensorStop&sensorStart.

But when switching to beamforming, it is very time-consuming. We found mainly the phase shifter is configured, which need send command 48(4 chip * 12 chirp) times to AWR2243.

TDM-MIMO will disable the phase shifter, only beamforming enables and uses it.

So i want to know whether the configurations of Phase shifter can be saved in AWR2243 instead of configure it each time?