Hello, I am using MMWCAS-RF-EVM and now I have two problems, 1. I need to transmit a large number of chirp in one frame, in theory, I can set numchirp=512,numloop=255, but once my configuration exceeds numchirp=12,numloop=128, the data will be distorted and the received signal will be severely distorted. I'm sending a lot of chirp. How do I configure it so that the data isn't distorted? 2. Frames will be lost from time to time, I set 1000 frames but only receive 900 frames, how should I configure to ensure that I do not lose frames?