This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: Start up problems

Part Number: IWR6843ISK-ODS


Tool/software:

I am having trouble running mmW studio for my IWR6843ISK-ODS, which is connected both to a DCA1000 data acquisition board and to my PC.  Specifically, when I start up mmW Studio, the program outputs a set of RSTD error codes and then dies.  I tried using the DCA1000 debugging handbook to sort out the issue, but cannot find the directories on my computer where the handbook says the RSTD files are located.  Question1: Is this a Windows 11 issue?  I saw an earlier thread where this possibility was raised, but no do definitive answer was given.  Question 2: If this is not a Windows 11 issue, how can I go about removing or working around the offending files so mmW Studio will start?  Question 3: If this is a Windows 11 issue, what are my options?  Thank you.