This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWRL6432: How to understand the value of compRangeBiasAndRxChanPhase

Part Number: AWRL6432

Tool/software:

Hi team,

I have one question on AWRL6432 about this command

compRangeBiasAndRxChanPhase 0.0 1.00000 0.00000 -1.00000 0.00000 1.00000 0.00000 -1.00000 0.00000 1.00000 0.00000 -1.00000 0.00000
In the userguide, this command is descripted like below:
The virtual antenna pattern of TI EVM and antennaGeo is like below:
If we choose BPM waveform, then the phase should be:
virtual antenna 1-3 are same as virtual antenna 4-6 or
virtual antenna 1-3 are opposite as virtual antenna 4-6.
 
But it seems the phase compensation of virtual antenna of 1, 3, 5 is set to 1, and virtual antenna 2, 4, 6 is set to -1.
Can you help me understand this?
Regards,
Shawn