Part Number: TMP61-Q1
Other Parts Discussed in Thread: TMP61
Tool/software:
Hello E2E Community,
We are considering the use of TO-92 packaged version of TMP61-Q1 for one of our remote temperature measuring use case with 3m long twisted pair cables.
I am seeking clarification about the following Figure 8-13 from datasheet about the errors.

Assume following as our configuration:
- Do NOT perform 1-point offset calibration
- Use Rbias 10kOhm +-0.5% (50ppm) [cannot use current bias configuration]
- Install RC Low Pass Filter with 15kHz cutoff
- We perform 1024 oversampling on our ADC for improving accuracy
How do we calculate the expected error typical & min/max from this configuration?
Is it a safe assumption the errors (min/max) are instantaneous errors & can be averaged out by oversampling?

Also, will performing 1-point calibration significantly improve the measurement accuracy?
Our expected accuracy is +/-2'C maximum.
Kindly guide with your best insights to speed up our design decisions.