This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMAG5273: Magnetic field values

Part Number: TMAG5273


Tool/software:

Hello,

I am working on capturing relay's (I have a relay from Zettler- 100A, 480VAC 55V, 690VAC) magnetic field through Hall effect sensor TMAG5273. Looking into datasheet of TMAG5273, I was trying to configure INT_Threshold register from the API ("uint8_t setIntThreshold(uint8_t threshold);")given in TMAG5273 library from Sparkfun. I didn't see any difference in my result. That's why I checked its register address and found the register address as 49h. But if I see 49h in TMAG5273 datasheet I get something like "MANUFACTURER_ID_LSB Register (Offset = Eh) [Reset = 49h]" which doesn't make sense. I appreciate if you can help in how to configure threshold to capture the correct magnetic field? and for what functioning the above API is used?