Other Parts Discussed in Thread: AWR1642, DCA1000EVM
Tool/software:
While Opening the mmwave studio, I am not able to see the window titled as RadarAPI as I was following the Ti mmwave training materials
I am also facing matlab runtime issue during startup , even after installing Matlab runtime engine 8.5.1v. also adding to the environment variables
Please see the below logs for your reference.
[22:08:27] [RadarAPI]: Status: Passed
[22:08:27] Matlab Runtime Engine is not installed
[22:08:27] [RadarAPI]: Starting Matlab Engine..
[22:08:27] [RadarAPI]: Error: The type initializer for 'MatlabPostProcGui.MatlabPostProcGUIClass' threw an exception.
[22:08:27] Trace:
[22:08:27] at MatlabPostProcGui.MatlabPostProcGUIClass..ctor()
[22:08:27] at AR1xController.frmAR1Main.InitMatlabPostProcEngine(String PostProcesspath)
[22:08:27] [RadarAPI]: Error: Error occured in Matlab Initialization
[22:08:27] [RadarAPI]: Matlab Engine couldn't be Started..
[22:08:31] [RadarAPI]: ar1.selectCascadeMode(0)
[22:08:31] [RadarAPI]: Status: Passed
[22:08:31] [RadarAPI]: ar1.LoadSettings('C:\Users\Sakthi\AppData\Roaming\RSTD\ar1gui.ini')
[22:08:31] [RadarAPI]: Error: Object reference not set to an instance of an object.
[22:08:31] Trace:
[22:08:31] at AR1xController.ScriptOps.getMatlabPostProcVersion()
[22:08:32]
[22:08:32] &&&&&&&&&&&&&&&&&&&&
[22:08:32] ***Script FAILED!***
[22:08:32] &&&&&&&&&&&&&&&&&&&&
[22:08:32] Exception message is:
[22:08:32] An attempt was made to load a program with an incorrect format. (Exception from HRESULT: 0x8007000B)
I am currently using mmwave studio 2.1.1.0.
I have interface AWR1642BOOSTODS with DCA 1000. I have also installed mmwave sdk mmwave_sdk_03_06_02_00-LTS-Windows-x86-Install