Tool/software:
When I run mmWave Studio, using a DCA1000 and IWR6843ISK and setup as follows: 4 Rx antenna, 256 A/D samples/chirp, 128 chirps, 8 frames. One of the four plots I select is the time domain plot (the waveform of the beat frequency). My question is: When I look at the time sampled beat frequency and calculate what frequency I expect to see based on using a corner reflector at a known distance, I get the correct frequency (knowing the chirp ramp rate). I want to know how the data is processed by matlab. Are a bunch of the chirps from each Rx antenna averaged together, and if so, how? Can I look at the matlab m file that does this? Where?
Thanks,
Larry