Part Number: TMCS1101
Tool/software:
Hi team,
If we calculate according to the datasheet, it seems that the smaller the input current, the larger the RSS total error will be, but are there any regulations regarding the maximum RSS total error?
When determining the specifications for the current detection unit, my customer ideally wants the error to be within ±5% from 0A to 15A. However, when calculating, the RSS total error exceeds 5% when the input current is less than 3A, so does the error specification need to be changed according to the current value?
Regards,
Taito Takemura