Other Parts Discussed in Thread: IWRL1432, IWR6843
Tool/software:
From the following post, it appears a stationary radar such as the IWR1443 is capable of mapping the surface of a large stationary target such as a pile of grain or the ground.
e2e.ti.com/.../iwr1443-surface-profile-with-mmwave-radar-sensor
Can you provide more information about this application? Is there an application note you can point me to or, better yet, could we arrange a call with an application engineer that is knowledgeable about this application.
The most common application for radar appears to be detecting moving targets, such as object detection for autonomous vehicles, or a single distance to a stationary target, such as level in a tank. I am interested in using a stationary radar to map distances to a large, potentially uneven, surface with enough precision to estimate volume of the target. The desired output would be a constellation of point representing the surface of a large stationary target. Is that possible with the IWR1443 using existing radar processing algorithms that would be available from TI? Is there a better radar chip for this purpose?