Tool/software:
Hi,
I want to ask a question regarding multiple objection detection in HECR for the same range and doppler index.
1. I want to if it is possible to detect multiple object in the same range and doppler index in HECR application or not? I tried to find information in "/ti/mmwave_mcuplus_sdk_04_02_00_01/mmwave_mcuplus_sdk_04_02_00_01/ti/datapath/dpc/dpu/aoaproc/docs/doxygen/html/index.html#HWA-AOA-start" but was unable to find any information. If it is enabled can you provide some description or documents where we can find this information.
2. In "\ti\mmwave_mcuplus_sdk_04_04_01_02\mmwave_mcuplus_sdk_04_04_01_02\ti\datapath\dpu\aoaproc\src\aoaprochwa.c" there is 'aoaHwaObj->dynLocalCfg.multiObjBeamFormingCfg.enabled" to set the multple object beamforming but it is parameter of TDM and not DDM. Does it work in DDM-MIMO case too.?
Thanks for your answer in advance.
Regards.