This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWAVE-STUDIO: version 2.1.1.0 getting error with unable to load DLL RadarLinkDLL.dll

Part Number: MMWAVE-STUDIO
Other Parts Discussed in Thread: IWR6843AOP

Tool/software:

Hi,

there have been a few posts in the past about this error, but the answers are inconclusive. When the mmWave Studio starts up, getting this error

[17:20:37] &&&&&&&&&&&&&&&&&&&&
[17:20:37] ***Script FAILED!***
[17:20:37] &&&&&&&&&&&&&&&&&&&&
[17:20:37] Exception message is:
[17:20:37] Unable to load DLL 'RadarLinkDLL.dll': The specified module could not be found. (Exception from HRESULT: 0x8007007E)

I verified that the RadarLinkDLL.dll is in two places in the directory structure

C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime

C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\AR1xController

The PC is a Windows 11 machine.

What is missing?

Complete log:

GM: Constructor
GM: Wed Sep 11 17:20:36 2024
RSTD.Transmit("/Settings")
[17:20:36]
[17:20:36] ### Running Startup script: "C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Startup.lua" ###
[17:20:36] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[17:20:36] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[17:20:36] Scripter ignored: Attempt to UnBuild() again or before Build.
[17:20:36] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[17:20:36] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[17:20:36] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[17:20:36] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[17:20:36] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[17:20:36] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[17:20:36] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\RunTime\\SAL.dll")
[17:20:36] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[17:20:36] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[17:20:36] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[17:20:36] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[17:20:36] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[17:20:36] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[17:20:36] RSTD.Transmit("/")
[17:20:36] RSTD.SaveSettings(): Settings saved to "C:\Users\gunts\AppData\Roaming\RSTD\config.xml"
[17:20:36] RSTD.Build()
[17:20:36] RSTD.SaveSettings(): Settings saved to "C:\Users\gunts\AppData\Roaming\RSTD\config.xml"
[17:20:36] RSTD.Transmit("/")
[17:20:36] RSTD.AL_Build()
[17:20:36] RSTD.AL_LoadXml()
[17:20:36] RSTD.Transmit("/")
[17:20:36] RSTD.AL_Init()
[17:20:36] RSTD.Clients_Build()
[17:20:36] GM: Init
[17:20:36] GM: Loaded 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\\LabClient.dll'
[17:20:36] GM: 1 Guest (s) init
[17:20:36] GM: 1 Module(s) init
[17:20:36] GM: 2 Tab (s) init
[17:20:36] RSTD.Client_LoadXml()
[17:20:37] [RadarAPI]: ar1.selectRadarMode(0)
[17:20:37]
[17:20:37] &&&&&&&&&&&&&&&&&&&&
[17:20:37] ***Script FAILED!***
[17:20:37] &&&&&&&&&&&&&&&&&&&&
[17:20:37] Exception message is:
[17:20:37] Unable to load DLL 'RadarLinkDLL.dll': The specified module could not be found. (Exception from HRESULT: 0x8007007E)

Thanks!

--Gunter