This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Request the source code for Drone Object Detection Application

Part Number: IWR6843AOPEVM

Tool/software:

Hi TI,

I have a project of using radar for drone object detection. The hardware i have is IWR6843AOPEVM.

I find that there is an example source code meeting the application requirements. That is in \radar_toolbox_2_20_00_05\source\ti\examples\Presence_and_Motion_Detection. However, this example source code doesn't support for IWR6843AOPEVM (the hardware I am using).

May you suggest how i can use the source code Presence_and_Motion_Detection or something with the same application for IWR6843AOPEVM.

Regards,

Dai Tran Quoc