This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: AWR1843

Part Number: AWR1843
Other Parts Discussed in Thread: AWR6843ISK

Tool/software:

 hi kaushik,

   i have few question reference to your clarification"

The values of the K0 set are derived empirically based on the expected SNR and are configured in the following file:

\MatlabExamples\4chip_cascade_MIMO_example\main\cascade\paramGen\module_param.m"

the attached screen shot has threshold scaling factor of 6.3 ( which is corresponding to SNR of 8 dB (converted into linear scale 10^(8/10)).

My question:

   How threshold factor of 6.3 is converted and Set as "CFAR_CASO_k0 = [5 3 ] ? can you confirm how these values are obtained?

regards,

mani