This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2214: Detection of human hand only

Part Number: FDC2214
Other Parts Discussed in Thread: FDC1004

Tool/software:

I have design challenge to make the LED camp with the human hand detection. Requirement mention below.

  • LED lamp has close body which is cover by the plastic part so no external exposed of electrical parts
  • Need to detect the human hand with the maximum range of 10-20 cm
  • Other object should not be detected

To achieved the requirement we come to know that the capacitive proximity sensor is the closet option.

Is FDC2214 suitable for that? 

Suggestions are welcome