Tool/software:
hello everyone,
I used four AWR2243 chips to cascade into a radar,and I found a problem.In the following different configurations, data reception is incomplete
chirps = 6, loop = 128 ,samples = 1024  only unit0 callback
chirps = 6, loop = 64 ,samples = 1024 unit0,unit1 create callback
chirps = 6, loop = 32 ,samples = 1024 unit0,unit1,unit2,unit3 create callback normally.
The maximum frame size limit for the AWR2243?