Other Parts Discussed in Thread: AWR1642, IWR6843, IWRL6432
Tool/software:
Hi,
I'm working on a project where I need to use the AWR1642 BOOST radar sensor to detect gestures and then use these gestures to move between screens on an ESP32-S3 ESP-Box. I’m looking for any sample C code or libraries that could help integrate these two components.
Has anyone worked on a similar setup? Specifically:
- How to process the gesture data from the AWR1642 and send it to the ESP32-S3?
- Any sample c/cpp code for handling gesture recognition on the AWR1642 since esp32 common base should be c/cpp?
- How to handle the communication between the AWR1642 and the ESP32-S3 for controlling the screen transitions?
Any guidance, examples, or documentation would be greatly appreciated!
Thanks!