This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: AWR2243 four-chip cascade design Slave 2 transceiver antenna has no data feedback

Part Number: AWR2243

Tool/software:

Dear TI engineers, hello!
       We are using AWR2243 to design a four-chip cascade radar. We have encountered a problem. Please help to solve it:
        At present, the transmitting antennas and receiving antennas of the three chips of our master, slave 1, and slave 3 can work normally, and each transmitting and receiving antenna has data. However, the three transmitting antennas and four receiving antennas of our slave 2 cannot work properly. The three transmitting antennas of slave 2 do not send waveforms, and the four receiving antennas of slave 2 cannot receive any signals. The antenna schemes of our four AWR2243 are the same.
       I checked that the master can normally generate 20GHZ LO signals (but we cannot detect whether slave 2 has successfully received the 20GHZ LO signal), and the synchronization signal (DIG_SYNCIN) is also normal, and the 40MHZ crystal oscillator signal is also available. The SPI communication of slave 2 in the software is normal, and there is a corresponding interrupt signal (SPI_HOST_INTR1). I checked that the power supply of the slave is normal, including NERROR_OUT, WARM_RST, and NRST. Judging from the current fluctuation, the RF function of slave 2 should not be successfully started, because when we turn on the transceiver antenna of slave 2, there is no obvious current fluctuation.
        How should we check the specific cause? Can the software monitor the status returned after the AWR2243 transmitting antenna or receiving antenna is successfully turned on?
      Looking forward to your reply!
      Best wishes!