Tool/software:
Hi Experts,
We're trying to use an AWR1642Boost Rev. module for research purposes. I can't seem to connect to the out-of-the-box demo in either functional or development mode. I'm able to flash the OOB demo in the mmwave_sdk_03_06_02_00 to the board in flashing mode. Further, when I try to use the Matlab TI toolbox again I'm able to flash but unable to connect in functional mode. Using mmwave_studio_02_01_01_00 in development mode I'm able to connect rs232, flash the eval firmware in the same folder(xwr16xx_masterss.bin for mss and xwr16xx_radarss.bin for bss), and connect over spi. However, when I try to power up RF I get:
[16:21:48] Status: Failed, Error Type: RESP TIMEOUT
[16:21:52] BSS Power Up async event was not received!
Basically, I haven't had luck with the awr1642boost module. Am I doing something wrong?
I looked through the forum last night and couldn't find anything similar, so I tried most of the suggestions that were somewhat related.
Please advise
Regards,
Josel