Other Parts Discussed in Thread: MMWCAS-RF-EVM,
Tool/software:
Hi All,
I'm working on a design that is a modificationof the MMWCAS-RF-EVM board.
I note as per the 'AWR2243 Cascade' document, that there must be a delay match between the 2x LO outputs of the master (FMCW_CLKOUT and FMCW_SYNCOUT), and the subsequent 4 outputs of the 2 Wilkinson splitters. This all makes sense.
I note from the Altium design that in particular the 'supplies' to the Wilkinson splitters are not length / delay matched at all, measuring in at 17.151 and 13.018mm for the lines on Layer 3 and do not look to be compensated by lengths on layer 1. Additionally, the delay measurement of each net AWR_1_FMCW_CLKOUT and AWR_1_FMCW_SYNCOUT differ by about 30 ps. I appreciate due to the net naming conventions, that each net delay comprises of sum of the source to, and both outputs from each Wilkinson divider, but I would have expected the total delay for each net to be equal?
Please could I confirm if there are any internal package delays that need to be taken into account when length matching FMCW_CLKOUT and FMCW_SYNCOUT traces?
Many thanks,
James