Part Number: AWR2243BOOST
Other Parts Discussed in Thread: DCA1000EVM, AWR2243,
Tool/software:
Hi all,
I am facing some weird errors while running the TI radar kit (DCA1000EVM and AWR2243B).
Everytime I try to use the mmwave studio in the connection tab I press RS232 Connect switch and I upload the BSS and MSS firmwares, and then when I press the SPI connect switch it shows some errors. I have tried changing the Power Supply and also tried restarting the Radar, but it does not work.
The SPI connectivity status remains always disconnected.
The error is :
[17:22:27] [RadarAPI]: ar1.SaveSettings('C:\Users\admin\AppData\Roaming\RSTD\ar1gui.ini')
[17:22:36] [RadarAPI]: ar1.ReadRegister(0xffffe214, 0, 31)
[17:22:36] [RadarAPI]: ar1.ReadRegister(0xffffe218, 0, 31)
[17:22:36] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_03_00_00_14\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\AWR2243_ES1_1\\radarss\\xwr22xx_radarss.bin")
[17:22:37] [RadarAPI]: Downloading BSS Patch RPRC Binary..
[17:22:37] [RadarAPI]: ar1.GetBSSFwVersion()
[17:22:37] [RadarAPI]: BSSFwVersion:(02.02.00.13 (07/03/20))
[17:22:38] [RadarAPI]: ar1.GetBSSPatchFwVersion()
[17:22:38] [RadarAPI]: BSSPatchFwVersion:(02.02.02.06 (12/08/20))
[17:22:38] BSS FW Download Success
[17:22:38] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_03_00_00_14\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\AWR2243_ES1_1\\masterss\\xwr22xx_masterss.bin")
[17:22:39] [RadarAPI]: Downloading MSS RPRC Binary..
[17:22:42] [RadarAPI]: ar1.GetMSSFwVersion()
[17:22:42] [RadarAPI]: MSSFwVersion:(02.02.02.00 (29/07/20))
[17:22:42] MSS FW Download Success
[17:23:18] [RadarAPI]: ar1.PowerOn(1, 1000, 0, 0)
[17:23:18] Status: Failed, Error Type: RESP TIMEOUT
[17:23:23] MSS Power Up async event was not received!
Please help me so that I can use it.
Thanks and regards,
Niladri