Tool/software:
Greetings,
I am working with a IWR6843ISK. I just downloaded and installed mmWave Studio. When I open it the following error pops up: Unable to load DLL 'RadarLinkDLL.dll': The specified module could not be found. (Exception from HRESULT: 0x8007007E).
The installation of the fdti drivers was successful and the so called RadarLinkDLL.dll is in C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\RunTime. I am only using the IWR6843ISK, I am not using any other devices such as the DCA1000 capture card or mmWave Dev Pack/ICEBoost
I have already tried the following in an attempt to fix the issue:
- Re-installing everything
- Using various different sources for the FTDI drivers, as well as those that come with mmWave Studio
- Downloading and installing different Microsoft Visual C++ Redistributable packages
- Booting up mmWave Studio while the IWR6843ISK is connected and while it is not connected
Thankyou very much for your help.
Best Regards.