Tool/software:
Hello,
I would like to inquire in detail about the questions in the thread(iwr1843-reference-temperature-for-txgaintemplut).
I have reviewed the document (spracf4) mentioned in the responses. It states that temperature sensors located near the TX and RX channels are used for boot-time calibration and run-time calibration, but there does not seem to be any mention of the temperature sensors used during LUT generation.
Regarding the IWR1834, please answer the following questions.
Question 1:
Is the average value of the seven sensors (TX0-2, RX0-3) used for boot-time calibration and run-time calibration? Does this mean the PM and DIG0, DIG1 temperature sensors are not used?
Question 2:
Is the average value of the seven sensors (TX0-2, RX0-3) also used for gain LUT generation? Or, is the Rx Gain LUT based on the average value of temperature sensors RX0-3, and the Tx Gain LUT refers to the temperature sensor values for each Tx channel to match the gain LUT software structure?
Question 3:
Are the PM and DIG0, DIG1 temperature sensors not used for the self-calibration function or any other BSS controls?
Best Regards,
Yasuaki