This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Inconsistent FPGA Boot – FPGA_DONE_LED Not Lighting, No Ethernet, Zero Files Captured

Part Number: DCA1000EVM
Other Parts Discussed in Thread: IWR6843ISK

Tool/software:

Hello TI Team,

I'm working with IWR6843ISK + DCA1000EVM and have run into a persistent issue that seems related to the FPGA boot sequence on the DCA1000EVM.

Setup:

  • Sensor: IWR6843ISK (Rev D)

  • Capture board: DCA1000EVM

  • Power Supply: 5V, 3A barrel jack (verified regulated)

  • Ethernet: CAT6 cable + static IP (192.168.33.30 for PC, 192.168.33.180 for DCA)

  • Software: mmWave Studio v2.1.0.0

  • PC: Windows 10, tested with and without USB-to-RJ45 adapter

This happened for 2-3 times:

- The FPGA_DONE_LED lights up

  • Ethernet port LEDs glow.

  • ping 192.168.33.180 only receives 1 packet

  • Device is recognized in Device Manager under "Network Adapters".

But now after restarting the FPGA_DONE_LED is not lighting up after pressing SW7.

What I have done:

  • Verified and tried multiple DIP switch configurations:

    • SW1: all OFF

    • SW2: tried both 6=ON, 8=ON and 6=OFF, 8=ON for EEPROM fallback

  • Pressed SW7 after clean power cycle with delays

  • Repeated test across two different DCA1000EVM boardsboth behave identically

  • Tried two power supplies (both 5V 3A)

Can you please help me in figuring out the problem here?