This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC2114: LDC2114EVM and GUI software 1.10.0

Part Number: LDC2114


Tool/software:

Continuing to the previous communication, I ordered new evkit and it has the same issues.

Device is detected and operational but any change will cause the evkit to disconnect after I set the CONFIG_MODE bit to 0.

There seems to be no change with the new evkit, operation remains the same.

  • Kari,

    I am sorry to hear you are having problems with the EVM & GUI.

    it looks like the LDC2114 EVM User's Guide has two possibilities for changing device settings. 

    Following the steps called out in section 4.6.2 allowed updates the CONFIG_MODE bit of the RESET register without the board disconnecting.

    Section 4.7 describes use of the Configuration page change device settings, which seems to work.

    Please let me know if you have any questions.

    John

  • Seems like there is something wrong with the access rights of the nw.exe that is causing these errors. When I installed the software to my home computer, it requested some right for Defender settings that are not allowed in my company PC I will continue searching someone who could help with this.

  • Kari,

    John is out of office right now.  Thanks for the update.  Hopefully, your IT department is able to provide the access rights required.  I am going to close this thread for now, but let us know if anything else is needed.