This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: Image loading failed: !!! Aborting flashing of specified files!!!

Part Number: IWR1443
Other Parts Discussed in Thread: UNIFLASH

Tool/software:

Dear ,

         I am try to flash bin file in my iwr1443 hardware. I done some changes in your high accuracy firmware. and project is build and bin is generated but i not able to flash the bin in hardware. The following error is showing in uniflash.

 

[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: Initialization complete.
[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: Flashing process starting...
[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: Connecting to COM Port /dev/ttyUSB0...
[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: Reset connection to device
[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: Set break signal
[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: Connection to COM port succeeded. Flashing can proceed.
[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: Reading device version info...
[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: ** 1 files specified for flashing.
[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: Checking file /media/abhijeet/data1/Abhijeet/NCR/FW/CCS/Server_Upload/high_accuracy_14xx_mss_V1.0/Debug/xwr14xx_high_accuracy_mss.bin for correct header for IWR1443.
[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: Header of /media/abhijeet/data1/Abhijeet/NCR/FW/CCS/Server_Upload/high_accuracy_14xx_mss_V1.0/Debug/xwr14xx_high_accuracy_mss.bin file indicates it is not a valid file to flash to IWR1443: 0xb55a03d1
[29/05/2025, 16:03:31] [ERROR] Cortex_R4_0: !!! Aborting flashing of specified files!!!
[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: Disconnecting from device on COM port /dev/ttyUSB0...
[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...
[29/05/2025, 16:03:31] [INFO] Cortex_R4_0: Instance deinitialized!

In code compose when i build the project the following result is showing on console 

Building target: "xwr14xx_high_accuracy_mss.elf"
Invoking: ARM Linker
"/opt/ti/ti-cgt-arm_18.1.5.LTS/bin/armcl" -mv7R4 --code_state=32 --float_support=VFPv3D16 -me -O3 --define=SOC_XWR14XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=DebugP_ASSERT_ENABLED --define=MMWAVE_L3RAM_SIZE=0x40000 -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=packed --abi=eabi -z -m"xwr14xx_high_accuracy_mss.map" --heap_size=0x800 --stack_size=0x800 -i"/opt/ti/ti-cgt-arm_18.1.5.LTS/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/control/mmwave/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/control/mmwavelink/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/adcbuf/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/crc/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/dma/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/edma/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/esm/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/gpio/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/hwa/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/mailbox/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/osal/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/pinmux/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/soc/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/uart/lib" -i"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/utils/cli/lib" -i"/opt/ti/ti-cgt-arm_18.1.5.LTS/include" --priority --reread_libs --disable_auto_rts --diag_warning=225 --diag_wrap=off --display_error_number --warn_sections --xml_link_info="IWR1443_high_accuracy_14xx_mss_linkInfo.xml" --rom_model --unused_section_elimination=on -o "xwr14xx_high_accuracy_mss.elf" "./config_edma_util.obj" "./data_path.obj" "./main.obj" "./mmw_high_accu_14xx_cli.obj" "./sensor_mgmt.obj" "../mss_mmw_linker.cmd" "../r4f_linker.cmd" -l"configPkg/linker.cmd" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/dma/lib/libdma_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/osal/lib/libosal_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/esm/lib/libesm_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/gpio/lib/libgpio_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/soc/lib/libsoc_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/pinmux/lib/libpinmux_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/crc/lib/libcrc_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/uart/lib/libuart_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/mailbox/lib/libmailbox_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/adcbuf/lib/libadcbuf_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/control/mmwavelink/lib/libmmwavelink_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/control/mmwave/lib/libmmwave_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/edma/lib/libedma_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/utils/cli/lib/libcli_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/hwa/lib/libhwa_xwr14xx.aer4f" -l"/root/ti/mmwave_sdk_01_02_00_05/packages/ti/drivers/spi/lib/libspi_xwr14xx.aer4f" -lrtsv7R4_T_le_v3D16_eabi.lib -llibc.a
<Linking>
Finished building target: "xwr14xx_high_accuracy_mss.elf"

/root/ti/mmwave_sdk_01_02_00_05/packages/scripts/ImageCreator/xwr14xx/out2rprc/out2rprc.exe xwr14xx_high_accuracy_mss.elf xwr14xx_high_accuracy_mss.bin 0x08000000
Parsing the input object file, xwr14xx_high_accuracy_mss.elf.
Appending zeros 0
Appending zeros 256
Appending zeros 88048
File conversion complete!
/root/ti/mmwave_sdk_01_02_00_05/packages/scripts/ImageCreator/append_bin_crc/gen_bincrc32 xwr14xx_high_accuracy_mss.bin
>>>> Binary CRC32 = ece2f52d <<<<
>>>> Total bytes in binary file 92372 <<<<

  • Hello Abhijeet.

    Please avoid making duplicate threads and please continue the discussion on the original thread here, as it looks like the conversation was incomplete.  I am closing this thread; please copy your question to the original thread to continue the discussion.

    Sincerely,

    Santosh