This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: 3 Transmit - not working- DCA1000 EVM & IWR6843AOPEVM

Part Number: IWR6843AOPEVM

Tool/software:

Hi,

I enabled 3 Transmit (Tx0, Tx1, Tx2) in Chirp tab, and set Start Chirp Tx: 0, End chirp Tx: 2; No. of chirp loops to 128 in Frame tab of mmwave studio . But I am getting only 128 chirps in adc data as well as  postproc plots. please see sensor config and PostProc outputs below. Post Proc should show 384 chirps instead of 128 chirps. Also adc data file is only 512 KB (same as one transmit antenna). 

thanks

Rafi