This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432AOP: GUI tool SysConfig

Part Number: IWRL6432AOP
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

It looks that the GUI tool SysConfig can be used for the No Flash boot via SPI interface.

Why doesn't it recommended?

<Described SysConfig settings>
-SPI Settings-
SPI Controller: xWRL6432 where this example is running
SPI Peripheral: xWRL6432 without Flash

-Setting Value-
SPI Mode: 0 (Polarity 0, Phase 0)
SPI Clock Frequency: 22 MHz

  • Hello.

    I'm a bit confused on what the question is here.  Are you asking about the SPI settings set in the application that is sent over the SPI interface?  Or are you talking about the SPI settings for the device without SFLASH?

    Sincerely,

    Santosh