This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: AWR2243 configuration with mmWave Studio

Part Number: AWR2243BOOST
Other Parts Discussed in Thread: DCA1000EVM

Tool/software:

Hi,

I am currently working on an application using the AWR2243BOOST in combination with the DCA1000EVM. I would like to know if it is possible to configure the AWR2243BOOST without using mmWave Studio or the DFP (Device Firmware Package), particularly in the following environments:

  1. Linux-based system, and

  2. Bare-metal processor environment (for real-time applications).

Is there any way to bypass both the mmWave Studio and the DFP, and still be able to configure and control the AWR2243BOOST for data acquisition and real-time processing?

Any guidance or recommended approach would be greatly appreciated.

Best regards,

Cedric