Other Parts Discussed in Thread: IWR6843AOP
Tool/software:
Hello,
I am experiencing the same issue for on application.
Part used: IWR6843AoP
SDK Version: 3.5.0.4
Firmware: OOB or the demo version.
Applicaiton: It is used for altimeter application to measure the distance to various grounds: Concrete, Grass, Wooden ship decks with metal frames underneath.
Observation: The Altimeter worked well against the concrete, wooden deck. When measuring against grass pads, there are geometries where the cloud point output (TLV 1 and 7) has detections with missing SNR or SNR values -1. This gap or missing SNR gap would varies between 0.2 to over a second.
The range CFAR threshold was set to 15 dB.
The frame is set to 100msec.