Part Number: IWRL6432AOPEVM
Other Parts Discussed in Thread: DCA1000EVM, , IWRL6432
Hello,
I am trying to set up the DCA1000EVM to work with the IWRL6432AOPEVM. I have been following along to this link: https://dev.ti.com/tirex/explore/node?a=1AslXXD__1.00.00.26&node=A__AZpB296-3QEz48rsFnFiOw__radar_toolbox__1AslXXD__LATEST. I have gotten everything to work. Now I am onto the subsection "DCA1000EVM mmWave Studio xWRLx432".
I have the pins and plug ins set up as in the image below in the instructions.

I have adjusted the setup lua file. Below are snips of my adjusted file.



I am now at the part where I am trying to run the mmWave Studio GUI with the 60Ghz lua file setup. Below is a snip of my GUI and the error message I am receiving.

I have tried going through the troubleshooting handbook for the DCA1000EVM. I have only installed the matlab runtime 8.5.1 version. The path defintion is defined as in the image below.

I have noticed that the link under the APPSS subsection in the GUI changes when I run the GUI. Here is what it shows currently after running it.

The link is supposed to be "C:\ti\MMWAVE_L_SDK_05_05_04_02\firmware\mmwave_dfp\rfevalfirmware\appss", but I am unsure if that is the actual problem.
Any and all help is greatly appreciated.
Thanks,
Travis