Part Number: IWRL6844EVM
Hello,
I've been using the IWRL6844EVM with the DCA1000 for about 1–2 months now, primarily for measuring water surface velocity.
Initially, I extracted the data from the .bin files (post-processed via mmWave Studio), and it worked quite well. However, 1–2 weeks ago, I ran into errors when launching the software due to a conflict between PC security settings and mmWave Studio. I had to reinstall both the software and the MATLAB runtime.
Since then, I’ve tried taking measurements again, but the point clouds extracted from the data no longer have the usual shape. Instead of forming straight lines, they appear as clusters of points.
Could the software reinstallation have caused this issue? Would remake the installion proprelly and maybe reflashing the board with the original pre-installed firmware help? If so, do you know where I can find the firmware file and how to perform the flash?
Thanks in advance !