Part Number: DCA1000EVM
Hi TI Team,
I am looking for some guidance regarding an issue I am seeing with my DCA1000EVM.
Issue
- The board is connected to a 5 V DC adapter, and the DCA1000EVM board and the LM26400YMHX (U1) regulator becomes too hot within a short time. We have been using this board and was working properly until last day.
I am sharing my observations below.
1. I have never connected a 12 V supply to the DCA1000EVM. The board has always been powered using 5 V DC barrel jack adapter.
2. The below point shows a short.
Multimeter observations (board powered OFF)
The following measurements were taken with the board powered off:
Component Continuity to GND Resistance across component F1 Both ends show continuity to GND. ~0.2 ohms D16 Both ends show continuity to GND. ~8.6 ohms C112, C126 Both ends of both capacitors show continuity to GND. ~8.5 ohms each C38, C39 Both capacitors show continuity to GND. ~6.2 ohms each C36, C37 Both capacitors show continuity to GND. C36: ~70.7 ohms, C37: ~60.4 ohms
Based on the above observations, could you please let me know if there are any additional measurements or troubleshooting steps that would help identify the root cause of this issue?
Also, does this appear to be a potentially repairable issue ?
Any guidance or suggestions would be greatly appreciated. Thank you!