I'd like for the FDC2112 to wake up my system when a hand approaches it. The application note SNOA940 suggests that this is possible, though the datasheet only talks about asserting the interrupt pin when the status register changes -- when new data is ready. Is there a way to set a threshold in the FDC2112 so that it only asserts its interrupt pin when there's a minimum capacitance level detected?