This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'd like for the FDC2112 to wake up my system when a hand approaches it. The application note SNOA940 suggests that this is possible, though the datasheet only talks about asserting the interrupt pin when the status register changes -- when new data is ready. Is there a way to set a threshold in the FDC2112 so that it only asserts its interrupt pin when there's a minimum capacitance level detected?
Hello John,
There is a trick to achieve this feature. You can specify an "offset" to be subtracted from the output data. If the net value is negative, it is an error and can trigger the interrupt. By tuning the offset, you can essentially set the threshold.
Regards,
Yibo
Interesting. It sounds like this would only apply to the FDC2112 and FDC2114 parts, since these are the parts with offset registers. Is this correct?
Once you generate negative data, does this trigger the CH0_WD_ERR flag (for channel 0)? If it does, it looks like I could fire the interrupt by setting the WD_ERR2INT bit. Does this make sense?
Yibo -- thanks for the detailed response. This will not work for the FDC221x parts right? Without an offset setting, I don't see how they'd generate an under-range error. The eval board I have has a FDC2214 on it though, and I'd have to come up with another way to talk to a FDC2112 in order to test this.