This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Noise in Current Measurement

Other Parts Discussed in Thread: LDC1000EVM, LDC1612

Hello,

I bought a ring coil in order to measure the current through a wire using LDC1000EVM.
I measured the inductance without any current and then with a constant current dynamic load.
For a given current, I can observe a difference between inductances but it generates a lot of noise.

Could you tell me how can I reduced the noise ?

Thank you for your help.

The reference of the coil is : here

An example if I have 1.5A

The assembly is :

  • Hi Mehdi,
    would you be able to use the LDC1612 instead of the LDC1000? It has an significantly improved noise level (and many other advantages).
    Also, what is the inductance and capacitance of your sensor?
  • Hi Mehdi,
    I moved your post to the Inductive sensing forum.
  • Hi Ben,

    thanks for fast response, we'll order this other EVM. I work on the same project as Mehdi. the inductance is 20uH and we added an 100pF cap, which may not be ideal. The noise we're experiencing is picked up from the environment, it namely happens when we move the coil, So I wonder if we cannot improve immunity, or add an LPF, maybe reduce the length of the sensor wire....

    Any suggestions there?

    Is there any documentation related to current measurement using this part ?


    olivier

  • Hello Ben,

    Thank you for your response.
    To add what Olivier said we have an other coil with an inductance about 13µH but it less sensitive than the 20µH.coil. It can not detect current less than 1.5A. 
    Is there a specific inductance value with a good sensitivity which can correspond to a current measurement between 1 and 6A ?

    Thank you for your help.

     

  • Hello Mehdi and Oliver,


    Thank you for evaluating LDC devices for your application.

    I have summarized and addressed your concerns below:

    • Noise Immunity: From the pictures of the setup you posted noise could be introduced into the measurement from multiple environmental sources.
    • Human interference (hand etc.) could introduce capacitive effects which will throw off the measurement.
    • Any metallic object in the vicinity of the AC magnetic field generated by the wound coil will in addition introduce noise.
    • The relative movement of the cable within the toroid will introduce noise in the measurement
    • To improve the robustness and accuracy of the measurement you should try to put the LDC device as close to the Toroid as possible. If longer cables are required please shield the cables.
    • Sensitivity: Just to do a sanity check; were the Rp min and Rp max values programmed correctly for each of these coils? Was the CFB cap chosen correctly?
      • For more information about programming the Rp min nd RP max values correctly refer to the following Application Note.
      • This CFB capacitor ensures stability of LC tank oscillation. At maximum inductance value, the amplitude on the CFB pin should be 1Vpp. If the capacitor value is too low, the signal will clip, thus resulting in an increase of noise. If the capacitor value is too large, the signal amplitude will be too low, which degrades measurement resolution.

    If you are still having trouble with the measurements, could you post scope shots from INA and INB to GND with and without the current in the conducting cable.

    I am not aware of any collateral already present for current measurements with LDC devices but we are here to provide any help you may need in getting your measurement up and running.

    Good Luck!

    Varn Khanna,

    Applications Engineer, Sensor Signal Path,

    Silicon Valley Analog,
    Texas Instruments,
    1-669-721-6138.

  • Hi Khanna,

    thanks for response :
    noise immunity : would you recommend shielding both wire with the same shield and connect the only on the EVm side?

    Sensitivity: we used a 100pF CFB cap and didnt change the Rp/Rf settings : we were hoping that we were close enough to the coil value of the EVM. We'll take a look at the AN.
    CAn you please make quick suggestions?

    thanks
  • Hello Oliver,

    I would have been more than happy to recommend register settings if this was a conventional LDC application but at this moment I do not have enough information to give you an accurate answer. Scope shots would be really helpful...

    The LDC1000EVM coil has an inductance value of around 20uH, so you might be better situated for the 26uH inductor then for the 13uH one with the default settings but it really just depends on the toroid.

    We have a few tricks to determine these settings, you can give them a shot.

    The FAQ section in general is a good quick reference for the LDC1000.

    Regards,

    Varn Khanna,

    Applications Engineer, Sensor Signal Path,

    Silicon Valley Analog,
    Texas Instruments,

  • Hello Varn,

    Thank for your response and for sharing the Application Note

    I have some questions about this :

    • We can determine Rp with this equation :

    But how is it possible ? Rp is in Ohm and L/(C*Rs) is in H/(F*Ohm). There are not the same unit.

    • And here it is assumed that C is already known but we have to determine the right value for the capacitance.
      How can we determine C ?
    • Why CFB pin should be 1Vpp if inductance value is maximum ? In the Application Note it recommends to have 4Vpp (page 5) 

    I have scope shoot from INA and INB to GND with and without current :

    • INA without current

    • INB without current

    • INA with 1.5A

    • INB with 1.5A

    I could notice that the frequency decreases a little when there is current but I don't how the scope can affect the programmation of Rpmin and Rpmax.

    Thank you

  • The equation does not appear. It's the equation 1 in the Application Note (page 3)
    Rp=L/(C*Rs)

  • Hello Mehdi,

    The equation you are referring to for Rp is frequency dependent so you will need to resolve it in terms of impedance.

    For choosing the capacitor, 

    The LDC1000 operates between 5KHz and 5MHz, I would use the manufacturer specified inductance of the toroid and choose a capacitor that puts the frequency in this range. Please use the following equation to solve for C:

    For the amplitude part, page 5 of the App Note is referring to the Sensor Signal Amplitude on INA and INB. Where as, when you are choosing the CFB cap you will be probing the signal on the CFB pin which should be 1Vpp at maximum inductance.

    These subtle points aren't obvious in the App Note and I will provide this feedback to my team. I apologize for the confusion.

    Thank you for posting the scope shots, please give me some time to provide you with some ball park register settings.

    Regards,

    Varn.

  • Thanks for answer. I just received the LDC1612 and will run test on it.

    In the meantime results on LDC1000 don’t look very promising (although we got rid of noise by magnetic shielding)
    - The inductance for a given current vary in time : making the measurement not reproducible
    - The curve inductance vs. current isn’t necessarily monotonic

    To illustrate this, please find attached the result found:
    - First tab from 0 to 2A – 2 sets of measurement showing different data, and different curve shape
    - Second tab from 0 to 6A showing non monotonicity

    Do you have any idea of why we see these behaviour ?

    Thank you
  • Thanks for answer. I just received the LDC1612 and will run test on it.

    In the meantime results on LDC1000 don’t look very promising (although we got rid of noise by magnetic shielding)
    - The inductance for a given current vary in time : making the measurement not reproducible
    - The curve inductance vs. current isn’t necessarily monotonic

    To illustrate this, please find attached the result found:
    - First tab from 0 to 2A – 2 sets of measurement showing different data, and different curve shape
    - Second tab from 0 to 6A showing non monotonicity

    Do you have any idea of why we see these behaviors ?

    Thanks
  • I had forgotten the result

    Please find the attachement.

    Resultat rogowski coil with shied.xlsx

  • Hello Mehdi,

    I apologize for the delay in getting back to you. Could you confirm that you are using a COG cap with a low temp co in your measurement?

    I would also be curious about if the toroid is self heating?

    I will look at the data you posted and provide additional notes by end of today pacific time.

    Regards,

    Varn.

  • Hello Khanna,


    I think i am using COG cap but I am not sure and I don't know if it is low temp. You can see in the picture the cap that I am using. This the only 100pF cap that we have currently.
    Could you know if this cap correspond to the test ? If you have a ref for capacitance in radio spare could you send me the link ? I will order it.

    You can see the reference of the toroidal coil with this link : Wurth Ferrite Toroidal Inductor
    The size seems to be too large so that the toroid is self heating.

    Could you tell why it is important to have a COG cap with low temp ? And how the cap can prevent the differents value of L for a same current ?


    Thank you.

    Mehdi

  • Hello Mehdi,

    Using a cap with a high temp co will cause the frequency to shift with minor temperature variations which will affect your measurement.

    For reference here is another e2e post talking about something similar.

    In addition the cap needs to be as close to the toroid as possible.

    I will try looking through Radio spare for an appropriate cap. But here is one from digikey, you just need to make sure the temperature coefficient of the capacitor is <+/-30PPM/C.

    Regards,

    Varn.

  • Hello Khanna,


    I found a cap with roughly the same spec in RS here. I will order it and run a test.

    But do you think the cap is the only reason of the diferent value of L for a given current ?

    Because when I started the measure with 0A, I have increased the current until 3A. I could observe an inductance value which decreases slightly over time. I have continued to increase the current until 6A and when returned to 3A, the inductance was completely different than the first value. I can reiterate the operation and I will observe a third value of L.
    Some times, the coil seems to be saturated when I returne to 0A,  the inductance value is very high and when I increase the current, the inductance fall.
    You can see the video to illustrate this "saturation". The image in the video is reversed.

    You can also see the result result below.

    Result Rogowski Coil with LDC1612.xlsx

    If you are any idea, please let me know.

    Regards,

    Mehdi

  • Hi Mehdi,

    your use case is not one that the LDC has been designed to do or that we have previously explored. While it is certainly interesting research, I'm afraid we are not able to support it. Thank you for your understanding, and good luck with the evaluation.