This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000 general questions

Other Parts Discussed in Thread: TDC1000

Some fantastic videos and info that helped clear up a lot for me. Currently still have two questions:

1) The TDC1000 can interface to two different transducers. You can have one transducer as a transmit and one as a receiver, but can you have two transducers, both independently transmit and receive at the same time (say on different tanks) and report that information to the processor?

2) The TDC100 is configurable through a SPI, is it also possible to program it in C or other language to create or customize features and is the programming code for the SPI available to use as a starting point for coding?

3) In the videos (very helpful) there were a number of transducers used. Are there any links to these, specifically the 1MHz waterproof sensor?

Thanks in advance. Any advice would be greatly appreciated.