https://e2e.ti.com/support/sensor/ultrasonic/f/991/t/539200
Hi,
As you said, i have attached have glued my transducer to the bottom surface of my plastic beaker.
1) It is still not giving me proper reading and the readings are different most of the time(mostly a very small value) .
2) Under parity enable condition it is giving me a very high value , in addition to that the clock_count1 bar is showing a zero and it shows a huge value in time 1 register (in measurement mode 2) which should not be so.
3) water level is not increasing when i add water.
case 1) At parity disabled
WHEN PARiTY WAS ENABLED THE GRAPHS AND SETTINGS WERE AS BELOW
Kindly help me with this.
Thank you ,
Noble.