Part Number: TDC1000-TDC7200EVM
Hello,
I´m using the TDC7200-TDC1000EVM and changed the band-pass frequency on it. The LNA in the receive path is switched to Resistive Feedback Configuration.
When the distance between the sensor and the object gets to big, I don´t get a stop pulse, because the signal is way too small. The threshold is already switched to 35mV and the PGA Gain is 21dB.
Can I just use a resistor smaller than 900 Ohm (where C42/C43 used to be) to increase the gain? Is there another way to increase the gain?
Thank you.