Other Parts Discussed in Thread: , MSP430F5529
Hello all,
I am using TDC7200EVM connect with MPS430F559. In TDC7200 datasheet, it says the resolution is 55ps. However, my measurement is very fluctuating. These are specs i used:
START: 1 MHz pulses, 50 Ohms, 1.65V, offset 850 mV, 10% duty cycle, phase 0 degree.
STOP: exact same with START
CLOCK: external clock 10Mhz from Signal generator (4V)
I attached the measurement file here, can somebody explain to me why it's jumping up to 100ns? Also, I expect to see 0 time difference between signals. Thank you.