Other Parts Discussed in Thread: IWR1443
Hi,
In IWR1443BOOST_RevA_Schematics, what are the pin number of the reserved pins (see picture attached). We find 9 reserved pin in datasheet.
Thanks in advance,
Christophe
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In IWR1443BOOST_RevA_Schematics, what are the pin number of the reserved pins (see picture attached). We find 9 reserved pin in datasheet.
Thanks in advance,
Christophe
AR1443EVM-010_schematics_revML1216.pdfparing IWR1443 EVM schematic, and the newly released IWR1443 RevA datasheet
pins on schematic IWR1443BOOST REVA, pins on schematic IWR1443 EVM 010, pins in datasheet IWR1443 RevA Fig4-1, notes
no pins on sht3, B1 , B1 - reserved, reserved pin FM_CW_SYNCIN1(not used for IWR1443) should be GND
no pins on sht3, B15, B15 - reserved, reserved pin FM_CW_SYNCIN2 (not used for IWR1443) should be GND
no pins on sht3, D1, D1 - reserved, reserved pin FM_CW_CLKOUT (not used for IWR1443) no connect
no pins on sht3, D15, D15 - reserved, reserved pin FM_CW_SYNCOUT (not used for IWR1443) no connect
no pins on sht3, G13, G13 - reserved, connect to GND or pull to GND w/resistor - Vpp only used for 1.8v secure parts, not used for IWR1443
no pins on sht3, P4, P4 - reserved, I2C_SCL see pin mux used on EVM- PMIC Control
no pins on sht3, R3, R3 - reserved, I2C_SDA see pin mux used on EVM- PMIC Control
no pins on sht3, R4, R4 - reserved, MSS_UARTA_TX - MSS Logger used in EVM
no pins on sht3, R5, R5 - reserved, BSS_UART_TX - BSS Logger used in EVM
I have included the old EVM schematic as well.
Regards,
Joe Quintal