Hi all,
I'm currently designing a device which will be used for functional near-infrared spectroscopy (fNIRS) and I have a couple of questions to find out if the AFE44xx series ICs is suitable for what I'm trying to do. The concept of operation is very similar to pulse-oximetry, but the spacing between the LEDs and photodiode is larger (> 2.5cm) and I'm going to be monitoring changes/oscillations in oxy- and deoxy-hemoglobin concentrations, rather than absolute concentrations.
- I will require approximately 8+ individual sensors. Is it possible to multiplex the SPI interface of several AFE44xx chips? What about the chips with an I2C interface? Could I possibly use an additional I2C multiplexer to control and sample each of the AFE44xx chips sequentially? I would be polling the averaged red/IR ADC values periodically.
- Is it necessary to use the CLK output of these chips to clock my microcontroller or processor? If I'm to use more than one of these ICs, I probably can't use a common clock for all of them due to how far they are spaced apart. Will there be significant downsides to operating without a central clock? The fundamental frequency of what I'm trying to measure is quite low (< 10Hz).
- Can the AFE44xx ICs also drive laser diodes? Since the spacing between the LEDs and photodiode would be relatively large, the attenuation of light will be higher. I might need the increased light intensity.
Thanks,
Robert