Other Parts Discussed in Thread: OPT8241
Hi,
From my previous question about TIC_CLK the answer mentions "a minimum clock period requirement of 15ns". That is 66MHz, so 48MHz is ok.
In another thread about OPT9221 Master Serial Configuretion it says "the max clock frequency used for reading the SPI flash is 40MHz".
Would it mean driving SYSCLK_IN at 48MHz is violating the requirement for startup from SPI EEPROM?
Thanks.