This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: Water level measurement and resolution

Part Number: IWR1443

Hi everybody,

I'm planning to use this sensor to realize a level measurement system for industrial application such as tank, vessels and open channels. In order to replace ultrasonic transducers, that usually have a 1mm resolution in a 15m range, I would like to know if it's possible to get the same performance. We strictly must implement a 2-wire loop powered instrument, so probably we will reduce the ON-time of this device in order to reduce the power consumption, and also the microcontroller will "live"in LPM for a consistent part of the measuring cycle.

thanks a lot